Dear Chris;
I bought the TMDSHVMTRPFCKIT with HVPMSMTR.In this sense, i am abit confused. Please could you make the some important points clear?
1- The relevant link gives us the information that the PMSM is from Anaheim. http://focus.ti.com/docs/toolsw/folders/print/hvpmsmmtr.html.
But, when the PMSM is delivered to me, i saw it from Estun.
2- The reason of buying the PMSM from TI is to know exact model knowledge of it. (P,R,L,Qm, B and J). Now, i have one motor but three suppliers.
The PMSM is described in
TI Website: EMJ-04APB22
Estun Website: EMJ-04APA22
Anaheim Website: EMJ-04APA22
Please could you tell me which is true?
3- Again, the motor parameters from TI Control Suit;
// Define the electrical motor parametes (Estun Servomotor)
#define RS 2.35 // Stator resistance (ohm)
#define RR // Rotor resistance (ohm)
#define LS 0.0065 // Stator inductance (H)
#define LR // Rotor inductance (H)
#define LM // Magnatizing inductance (H)
#define POLES 8 // Number of pole // Number of poles
// Define the base quantites
#define BASE_VOLTAGE 236.14 // Base peak phase voltage (volt), Vdc/sqrt(3)
#define BASE_CURRENT 20 // Base peak phase current (amp), Max. measurable peak curr.
#define BASE_TORQUE // Base torque (N.m)
#define BASE_FLUX // Base flux linkage (volt.sec/rad)
#define BASE_FREQ 200 // Base electrical frequency (Hz)
and from the Anaheim and ESTUN are not compatible with eachother.
Please could you tell me which is true?
In order to realize the Project, i need to know the exact values of the motor parameters. For this reason, i can not start the work yet.
I should be very grateful if you give me exact motor parameters soon.
Best regards.