This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRINSPIN: Where is the voltage and PWM limit setting in the motorware?

Part Number: TMDSHVMTRINSPIN
Other Parts Discussed in Thread: HVPMSMMTR,

Hello,

I have TMDSHVMTRINSPIN ,HVPMSMMTR.

I build Lab5b and it works well.

But when I watch the gMotorVars variable in Watch Window, MotorVars.VdcBus_kV value is 0.307(it means 307V)

I know that the rated voltage of HVPMSMMTR is 200V.

Is there any problem with running motor at 300V?

Where are variables related to voltage and PWM limits?