Tool/software: Code Composer Studio
Hi
according to motorcontrol_sdk hal.h
"//! \brief Defines the gpio for the enable gate of DRV device
//!
#define HAL_DRV_EN_GATE_GPIO 28
"
is gpio 28 for switch enable?
if yes wy in hal.c it is not mentioned?
// No Connection
GPIO_setMasterCore(28, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_28_GPIO28);
GPIO_setDirectionMode(28, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(28, GPIO_PIN_TYPE_STD);
Kind regards