• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » C2000™ Microcontrollers » C2000 32-bit Microcontrollers Forum » All Tags » F28027
Share
C2000™ Microcontrollers
  • Forums
  • Announcements
  • E2E Wiki

Browse by Tags

C2000™ Microcontrollers

Welcome to the C2000™ Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
F28027
  • 28027
  • 28035
  • 28335
  • 2833x
  • ADC
  • bootloader
  • C Programming Language
  • C2000
  • C28x
  • CCS
  • CCS v4
  • CCSv4
  • Code Composer 4
  • Code Composer Studio
  • ControlSUITE
  • digital motor control
  • ePWM
  • eZdsp TMS320F28335
  • F28035
  • F2812
  • F28335
  • F2833x
  • F28x
  • F28xx
  • flash
Related Posts
  • Forum Post: Re: TMS320f28335 FOC with motor control library

    vsi-pete vsi-pete
    Dear hello84, I suggest you try VisSim/ECD. It is a block diagram language for embedded control targeted at TI C2000 devices. It has a complete motor control block set that allows off-line simulation, automatic C code generation and CCS compile. It will select the proper TI motor control library for...
    on Apr 28, 2009
  • Forum Post: Re: PICCOLO microcontroller (F28027)

    vsi-pete vsi-pete
    Hi Gaston, I don't think that RTDX supports the XDS100 ( http://tiexpressdsp.com/wiki/index.php?title=XDS100#Q:_When_using_DSP.2FBIOS_and_the_Real_Time_Analysis_setup_for_RTDX.2C_I_get_the_cpu_graph_and_real_time_logs_updating._Does_this_mean_RTDX_is_working.2Fsupported_on_the_XDS100.3F ) The Piccolo...
    on May 19, 2009
  • Forum Post: How to trace program execution flow before emulator halts voluntarily or involuntarily?

    Michael Fang Michael Fang
    I'm running my application from SARAM on Piccola Experimenter Kit with F28027 controlCARD. (CCS version: 3.3.81.28; Integrated Development: 5.98.0.393.) My application stops running with dissassembly window showing: 5 ESTOP0 . PC contains the value 03FF5F1. Call Stack Window only shows "03FF5F1"...
    on Jul 31, 2009
  • Forum Post: Piccolo USB controlStick communicates with PC via SCI?

    Silvan Huang Silvan Huang
    Hi, everybody! Can I use the FTDI on picolo usb stick as a dual rs232? I'm working on piccolo usb controlStick to build a prototype. The F28027 recieves a sampled value from ADC over SPI at the rate of 60kHz. These values have to be collected for further analysis. I wonder if it is possible...
    on Aug 19, 2009
  • Forum Post: 2802x v1.00 header files and flash api v1.00

    maldrich maldrich
    Hi guys, I am evaluating the control stick (F28027) and Matlab R2009b code generation tools. To properly evaluate my projects and example projects, I'd like to build based on what mathworks recommends. That being said, I am looking for the installers for both these: C2802x v1.00 header files...
    on Sep 25, 2009
  • Forum Post: Accuracy of TMS320F28027 internal clock?

    Janne Janne
    I can't find any info about the accuracy of the internal clock in the datasheet. /Janne
    on Sep 30, 2009
  • Forum Post: Clock synchronization

    andreas von kaenel andreas von kaenel
    Hi Folks I have an application with 3 TMS320F28027 (Slaves) and 1 ARM Cortex M3 (Master) Processor. For measurement reasons, it is critical, that the 3 Slaves run on a synchronized clock. The Piccolos are using their internal oscillators - no external crystal available. I would like to modulate the...
    on Dec 15, 2009
  • Forum Post: C Programing Language Doccumentation

    Peter C Peter C
    Hello everyone I recently acquired a F28027 Piccolo USB Stick, and i find it to be a great development platform. However, I do have a problem, which i guess relates more to the actual programming than the piccolo itself. Where is, if it exists, the documentation regarding the implementation of...
    on Jan 18, 2010
  • Forum Post: Verified: F28027 programming with Spectrum Digital XDS510 USB

    maldrich maldrich
    Hi, CCS Configuration: F2808 XDS510USB Factory Board, driver f2808_xds510usb.ccs GEL File: F27027.GEL Version 3.30.4 Matt
    on Jan 21, 2010
  • Forum Post: multiple fir 16 module usage on f28027 Piccolo

    Giovanni Perrino Giovanni Perrino
    Hi everyone. I'm using fir16 module on sprc082 library downloaded from this site. I don't understand if I have to create, in order to filter with the same coefficients two differents variables, two different memory sectors for these variables. More specifically, could I create a memory section...
    on Feb 2, 2010
  • Forum Post: F2802x SCI external pins

    ulu ulu
    In Piccolo Data Manual (SPRS523D) Table 2-2, there are 3 pairs of SCIRXDA/SCITXDA listed (mapped to various GPIO's). But there is only one SCI module in the DSP, I do not know how to decide which pins to use for tx and rx. Please show me some pointers. Thanks in advance. ...ulu
    on Mar 17, 2010
  • Forum Post: Creating File CCS v3.3 with F28027 controlCARD

    Michael Blankson Michael Blankson
    Dear all I'm creating file in CCS ver3.3 using F28027 controlCARD. But there are a lot of problems with linker command. Is anyone knows how to create files and how to change the link command file so, I can create a file. My main file: void main(void) { file = fopen("Textfile...
    on Apr 8, 2010
  • Forum Post: SWITCHING REGULATOR USING 28027USB

    salil desai salil desai
    HELLO I'M TRYING TO BUILD A SWITCHING REGULATOR USING THE F28027USB CONTROL STICK....I AM DRIVING A FULL MOSFET H-BRIDGE USING COMPLEMENTRY OUTPUTS FROM PWM1A AND PWM1B SINEWAVE PWM AFTER BOOTSTRAPPING...I'V IMPLEMENTED A VERY CRUDE SOFTSTART BUT IT WORKS...ONCE THE MOSFETS START SWITCHING AT...
    on Apr 12, 2010
  • Forum Post: PICCOLO microcontroller (F28027)

    DHARMRAJ GHODKE9821 DHARMRAJ GHODKE9821
    I am developing three phase power factor corrected AC to DC and DC-DC converter using PICCOLO microcontroller 320F28027, I want to use the motor controller library functions available for F2808 , like PID, sine, cosine, synchronous frame transformations ( park, ipark, clarke iclarke etc.), can somebody...
    on Feb 16, 2009
  • Forum Post: Propagation delay

    Michael Blankson Michael Blankson
    Hi all I need some technical help. What is the propagation delay in the DSP-TMS320F28027 ( Piccolo series ) and ADC chain? I need this information for my hardware design and also for my simulation. Thanks Michael
    on Apr 29, 2010
  • Forum Post: TMS320F28027 - ADC Interrupt Problem

    Johannes Dröge Johannes Dröge
    Hi verybody, I am trying to use the ADCINT on my TMS320F28027. It just wont work. This is the code I use to setup the interrupt: ADCInit(): EALLOW; AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; // use internal band gap reference AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // power up band gap AdcRegs.ADCCTL1.bit...
    on May 17, 2010
  • Forum Post: Re: Regarding LCD interface..

    challu challu
    Thanx for reply,I am using F28027 and want to send data through GPIO pins 0-7,there my doubt is can we send data through GPIO and which registers i want to use either GPXDAT or GPXSET registers.here i want to interface to graphic LCD.
    on Jun 8, 2010
  • Forum Post: CCS can run program out of RAM, but can't write / erase the flash on F28027

    Freddy Gauss Freddy Gauss
    I built a couple boards using the TMS320F28027. It shows up under CCS, I compile, run, and step through the code in RAM. But I cannot flash anything into the chip, nor can I erase the flash. Has anyone ever had this problem? This is not the first F28xx board I've built, but it's the first...
    on Jul 15, 2010
  • Forum Post: PiccoloF28027 SCI Echoback Example with 115200Baud

    Stefan Fischer Stefan Fischer
    Hi, i try to run the Piccolo Echoback Example with 115200Baud but i see nothing on my Hyperterminal (i also set my Hyperterminal setting to 115200)? When using 9600 Baud everything works fine. For 60MHz with 115200Baud i calculated my Sci Period Value with the formula : BRR=(LSPCLK_FREQ/(SCI_FREQ...
    on Jul 30, 2009
  • Forum Post: F28027 ADC external voltage error (triggered_ADC example)

    Ziyaad Jassiem Ziyaad Jassiem
    Hi, I'm fairly new around these parts and i'm having my first encounter with a TI product , the f28027, and i'm really eager to get this simple yet frustrating issue with the ADC solved. So im using the example project, TriggeredADC, and i have just connected an external voltage to...
    on Sep 16, 2010
  • Forum Post: Piccolo Continuous ADC example

    Lukas Pariza Lukas Pariza
    Hello, I think I need your help. I can't find another examples for my f28027 Piccolo ControlStick at this TI's web. To be specific, I need the ADC-ContinuousADC example project which some information about I found here: www.ti.com/f28xgetstarted Also the another example projects would...
    on Jan 1, 2011
  • Forum Post: ePWM, Trip zone and analog comparator

    JHi JHi
    I have set up the comparators in a way that when low over current occurs it will give me an interrupt which I handle. If there is a bigger overcurrent PWMs will be disabled and again interrupt occurs. The problem is that how can I configure the interrupts and everything so that I get only one interrupt...
    on Jun 23, 2010
  • Forum Post: ControlStick Stand-Alone Run?

    Qian Cheng Qian Cheng
    Hi, everybody I am new to TI's C2000 processor. There is no problem in runnig the example project of controlStick both in RAM and in Flash. But I want to let the controlStick run automaticlly. That is that after I plug the controlStick into the USB port, the processor can run the programme in...
    on Oct 12, 2010
  • Forum Post: Continuous AD conversion with F28027

    Henrik Karlsson Henrik Karlsson
    Hi, I'm using a Piccolo ControlSTICK (with a 28027 DSP) and are aiming to sample a signal at highest possible sample rate (4.6Msps). However, I have quite a lot of trouble when configuring my ADC. First off, I get the feeling that the highest sample rate, 4.6Msps, might be very optimistic....
    on Feb 10, 2011
  • Forum Post: Problems with the ADC function in the DPLib

    MD58785 MD58785
    Hello, I have some problems with the ADCDRV_1ch funtion. I'm using the DPLIB v3.1 on a piccolo controlSTICK with the blank-template file. The PWM works fine so far. I've added the following lines to set up the ePWM trigger: EALLOW; EPwm2Regs.ETSEL.bit.SOCAEN = 1; EPwm2Regs...
    on Feb 22, 2011
1234
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use