As reported in another post by a user, the F28027F controlCARD was not functioning correctly with the DRV8312 kit for InstaSPIN-FOC projects.
While the drv files in
sw\drivers\drv\boards\drv8312kit_revD\f28x\f2802x
are correct, the .cproject files that load the project in CCS are pointing to the drv files associated with the drv8301 board
Somehow this error was introduced in versions _10 and _11. It did NOT effect _09 and it will be corrected in _12 which will release end of February.
If you need to patch the error in the meantime it is a simple find & replace
Find: 8301
Repace With: 8312
In each .cproject file (open with text editor) in each proj_lab## folder at:
sw\solutions\instaspin_foc\boards\drv8312kit_revD\f28x\f2802xF\projects\ccs5\