I've got our motor to track positions in lab13b and it works great. If I understand correctly lab13a holds 0 position and lab13b accepts set point which then go though SpinTAC Move. What I would like to do is to track arbitrary positions as they are being generated. Imagine position x(t) = sin(2*PI*f*t) where t is the time. Without the knowledge of the form of the trajectory (only knowing its current and previous values), what is the best way of achieving this task? Is there a way to quickly achieve this in either lab13a or lab13b to continuously change the setpoint?
Thanks,
Sina