In lab13a the motor holds position at zero, so that we can set the bandwidth to achieve the desired tightness. I realized that while the motor is holding position if I apply a torque to the motor, the resiting torque increases (expected behavior) but only up to a certain point and then the motor gives and becomes free to spin. no changes in state or error codes is observed. Is there a reason for that? In my opinion the ideal behavior is to increase the torque up to MAXtorque (or current) and then simply saturate at that value. Is there an easy way of achieving that goal?
Thanks,
Sina