I'm trying to create a new project using InstaSPIN MOTION and Motorware 13. I'm coming across some problems with the CTRL module. For one thing the fields in _CTRL_Obj_ in the float version don't match up with the fields in the 32b version used in the labs. Also, some of the function's parameters are different.
Before I delve into it further, I noticed that the headers on the files in the float directory ( sw/modules/ctrl/src/float/ ) don't have the same headers as the other files. Is it possible that an incomplete version of these files was accidentally included in MotorWare 13? Is there something else that I'm overlooking?