Dear all,
I am using TMS320F28069F controller and motorware13 example implementation for AC induction motor 415V/50Hz system. I implemented lab examples(1-10) in my custom board.
I have some question related FOC.
-
My USER_PWM_FREQ_kHz = 5khz, and motor in running condition, then in one of my function require change decrease this frequency upto 2.5khz with 0.1 decrease factor in motor running condition. Is it possible in insta spin FOC? How?
-
Can I change USER_FORCE_ANGLE_FREQ_Hz from 1 to 0.5Hz?
-
Can I change USER_FORCE_ANGLE_FREQ_Hz in motor running condition? How?
-
What I have to do if i want to change some parameters(guserpara) from USER_setParams() function parameters in motor running condition?
-
Can I change from torque control to speed control and speed control to torque control during motor running condition? How?
-Suprit