Hi,
I've just successfully ID a 810KV hobby motor, that I intend to use for a quadrocopter. I am seeing some strange behavior that I dont know how to fix.
When I test the motor, I am able to speed it up to 11 000 RPM. But when I install the blade on the motor, the motor goes only to about 4000 RPM. The current is still below the limiting current, but I noticed that the torque is quite high around 10 000 Nm.
Is there a limit to the torque?
4532.user.hThe user.h is attached.