Hi,
I changed to libraries and the compiler option from softlib to FPU32. And now I have a strange problem.
I got the following warning:
This project contains unresolved buildable linked resources. It might not build as expected.
That is a bit short on information.
If I run the problem the following occur:
gMotorVars.Kp_Idq -128
gMotorVars.Ki_Idq 0
gMotorVars.VdcBus_kV 0
The motor doesn 't run and no error messages. Except 2002: Position error exceeds maximum
If I change it back to softlib everything work fine.
What I have to do to make it run in FPU32?
edit: Why do i need FPU32? Because Controlsuite only supplied usblib.lib in FPU32.