Hello,
I have some questions about speed reversal.
At start up, it is possible that that my motor run at the reverse direction I need. So I need to make a fying start and then a speed reversal.
On the first project with instaspin, inertia was quite low and this was working correctly, but now we have a motor with a high inertia and some time, the motor "stall" around zero RPM and oscillate.
Regarding : SPRUHJ1F, the following set up must be made:
• Enable offsets recalibration; described in Section 14.1.1.1.
• Enable stator Rs recalibration; described in Section 14.1.1.2.
• Disable forced angle; described in Section 14.1.1.3.
• Tune speed controller to avoid motor stall; described in Section 14.1.1.4.
• Tune voltage feedback circuit; described in Section 14.1.1.5.
But for a flying start, the offset and Rs recalibration are impossible.
During speed reversal, the speed will reduce from negative to positive and during a while, the speed will be too low to be identified (under USER_ZEROSPEEDLIMIT). So during this time, how thas it work without the force angle?
Another question is regarding this force angle, in a previous post Chris wrote this :
FORCE_ANGLE_FREQ > 2 * (USER_ZEROSPEEDLIMIT * USER_IQ_FULL_SCALE_FREQ_Hz )
This seems to be a problem for me because USER_ZEROSPEEDLIMIT is linked to HW scaling and flux of the motor and regarding test I have done, FORCE_ANGLE_FREQ is linked to inertia (frequency must be lower for a high inertia motor). So It seems difficult for a high inertia motor to respect what Chris wrote.
Regards.
Manu