Gautam Iyer said:Officially CCSv3.3 is supported but this version is no more available for download on TI website. CCS v4 too is supported but proper documentation is unavailable.
I've also heard the news that Matlab is working to bring back the support for C2000 controllers that would be compatible with CCSv6. Not suare, when!
Regards,
Gautam
Gautam,
Thanks for the help.
I have another question: Is it possible to make use of the InstaSPIN-Motion control in my Simulink model? The model contains the desired speed of the pedals of an electric bike, from which the needed motor speed can be calculated (making use of the current speed of the pedals, the used transmission and the losses). So this calculated desired motor speed, which is constantly changing and calculated in real-time, should be the input of the InstaSPIN-Motion module.
Do you have an idea of how to do this? Or would it be necessary to write the code for this directly in CCS?