I just purchased the DRV8312EVM kit (Rev D) and got it working with the pre-flashed image, with the included 24V 4,000 RPM motor, and with a sensorless trapezoidal control mode via DRV8312GUIv5 on my PC.
I am now trying to build a simple application to drive a different 3-phase sensorless BLDC motor (24V 40,000 RPM). All I care about is if the speed can be controlled to within 10% of what i nominally set.
I am new to this type of motor control; so this is probably a pretty basic question:
(1) Where in the GUI_project source code do I need to make changes to support the different motor?
For now I've avoided InstaSPIN (opting for the basic GUI control instead) because it wasn't pre-flashed and it seemed more complex for my current sensorless needs. Thanks for your time/help.