Inside the DRV812 development kit - USB stick came two GUI softwares: one of which was DRV8312GUIv5, which works perfectly and runs the kit's motor. The other however, InstaSPIN-BLDC_GUI_DRV83xx_v104 does not seem to run the kit's motor at all. All else the same.
I am using PMSM sensorless mode to move the motor. I would like to use InstaSPIN-BLDC_GUI_DRV83xx_v104 GUI such that I can control the speed using %duty cycle.