posted on another forum, and moved here:
Now another question please, the motorware GUI is working now.
However I have one board C2000 - F28027 (without the ROM that have all features)
I have understood that I have also files in this version that can run 3-phase motor sensorless.
I would like to get a working example - in which I define very simple inputs, and the SW will run DRV8301 according to this input (e.g. RPM, Accelaration etc.)
Do I have somewhere a working example (that compiled clean) ?
Also about GUI - do I have tools for GUI ready - so I can transfer data through a GUI that I am building as inputs for the CPU?
Also another example that just make the correct PWM (for 3-phase motor, usning TI ready sensorless libraries) for mosfet (without DRV8301) - meaning just GPIO out, with TI instant-Spin technology?
Thanks,
Roee