Hi,
I am new can some one please help me with these questions:
1. I have also kit TMS320F28027F that is working with MOTORWARE GUI - can I burn the code to this chip and make it run without the GUI - and use my own fix settings? - if yes how do I define it and do this?
2. Can I use some code to TMS320F28027 with DRV8301 (no F) - and control DRV8301 - there is no example ready to this chip, and I don't know yet how to convert the examples from another chip to this chip?
3. Does any one have any ready code that can spin 3-phase motor with DRV8301 and again the chip is regular (TMS320F28027)? or some example to "f" version without GUI?
4. How does the GUI transfer parameters to the chip? - is it UART or other protocol?, how can I build GUI myself to do this?
Any answer to even to one of these sections will help me.
Thanks,
Roee