Hello,
I am trying to use the motorware proj_lab_05g with an inverter that I already have. I used the example program 5g and made the appropriate changes (like the ADC channels and full_scale_voltage etc.).
However, this does not seem to work correctly. When I start the program and I put the System and Identify flags to 1. The CtrlState and EstState go to the OnLine state and stay there. Est does not go to the RoverL state. And I have a PWM signal with 50% duty cycle on the output.
Can someone tell me what I could be doing wrong? I am using the F28069MPZT card and Motorware13.
Udai