Hi
I am trying to run the BoostXL drv8301, that came with my LaunchPadXL F28027F, from an F28069MISO controlCARD that I recently purchased.
Setup
BoostXL DRV8301 board
11.1v LiPo
Anaheim BLY172S motor that comes from an 8312 Dev kit
F28069MISO controlCARD w/ docking stn. From C2000 Dev. Kit
USB to both docking stn. and controlCARD
On the controlCARD I’ve uploaded the Poject_Lab5c from the DRV8301_kit.RevD for the 28069M
I need to know if I have the boards connected properly. In the DRV8301 SPI tab of the MOTION GUI the SPI Working LED is green but the Rx Working is red, also the FETLC_OC is red(all others are green).
BoostXL DRV8301 F28069MISO controlCARD
3.3v J1.1 3.3v header
Fault J1.3 GPIO 28
OCTW J1.4 GPIO 29
SCLK J1.7 GPIO 18
GND J5.2 GND header
DC-V-FB J5.3 ADCIN-A7
VA-FB J5.4 ADCIN-A3
VB-FB J5.5 ADCIN-A1
VC-FB J5.6 ADCIN-A0
IA-FB J5.7 ADCIN-B1
IB-FB J5.8 ADCIN-B3
IC-FB J5.9 ADCIN-B7
GND J2.1 GND header
SCS J2.2 GPIO 19
SDI J2.6 GPIO 16
SDO J2.7 GPIO 17
EN-GATE J2.8 GPIO 6
DC-CAL J2.9 GPIO 7
PWM-AH J6.1 GPIO 0
PWM-AL J6.2 GPIO 1
PWM-BH J6.3 GPIO 2
PWM-BL J6.4 GPIO 3
PWM-CH J6.5 GPIO 4
PWM-CL J6.6 GPIO 5
When I try to identify the Anaheim motor from the FOC tab I get PWM's to the drv8301 but nothing out of the drv8301 PWM lines. The lab is designed for inertia identification, however I get an error code of 2004.
Thanks in advance,
Ben