Hi.
I need to design a new PCB to control 4 BLDC motors.
The 4 motors are 10A 36V maximum.
The old design we use has only 2 motors and it uses the TMS320F28335.
The maximum performance of the motors is 1 turn 360Deg CW and 1 360Deg CCW cycles in 20Hz.
My questions are:
1) Could I use the InstaSpin library to control all 4 motors with the same MCU and get the performance needed?
2) What is the most suitable MCU?
3) What evaluation boards are recommended to best evaluate the new design
Thank you.
David.