LAUNCHXL-F28069M is now available for immediate shipment.
- $25 LaunchPad with TWO sets of BoosterPack connectors
- Dual encoder headers and isolated CAN
- InstaSPIN-FOC and InstaSPIN-MOTION support (or use for non-InstaSPIN development as well)
- MotorWare projects for both sets of BoosterPack BOOSTXL-DRV8301 connectors individually
- Future MotorWare release will include projects with the single LaunchPad controlling both motors (summer '15 release)
- Development Partners like The Mathworks/Embedded Target and Altair/VisSim are already demonstrating dual motor operation using their own software
Initial Position Detection using High Frequency Injection (IPD_HFI) Library
- First release with initial example project on DRV8301 EVM (not BOOSTXL) using F2806x
- Future releases for other inverter hardware and F2802x and F2805x
- You can port the projects yourself as well
- New projects with write-ups in the Project & Labs User's Guide
- proj_lab20: example of slightly different CTRL code format, with PI controllers in CTRL and FOC/Transforms in mainISR
- proj_lab21: implementation of IPD_HFI with InstaSPIN-FOC (torque mode), including new AFSEL function to transition between IPD_HFI and FAST.
- future projects will include velocity control example
- Notes for IPD_HFI
- It is not "insta". It requires manual tuning (using a current probe is ideal) to select the proper values.
- It will not work with all motors. A certain amount of saliency (based on the rotor construction) is required.
- Please review the Projects thoroughly.
MotorWare Updated to version 1.01.00.14
- Support for new LaunchPad
- Support for new InstaSPIN-FOC based IPD_HFI projects (proj_lab20, proj_lab21; initially for DRV8301 EVM and F2806x)
- Updated sw\drivers to align with additional driver work being done across TI MCU