Hi,
I am trying to perform a current control for a BLDC motor. Can I take a feedback from the DRV and hookup to the ADC port of the DSP to complete the current control loop of the DSP.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am trying to perform a current control for a BLDC motor. Can I take a feedback from the DRV and hookup to the ADC port of the DSP to complete the current control loop of the DSP.
Thanks
Thanks for your reply , in order to be more precise on buying the right product please have a look at the following details of my problem. I think with this info you will be able to precisely advise me the DSP and the DRV which I should use to achieve the project objectives.
Actually I have four 12 volt maxon BLDC motors, which are coupled to the linear actuators through gears, . For clockwise rotation maximum displacement is 5mm.For anticlockwise rotation maxim displacement is -5mm.The ultimate goal is linear displacement control.The linear Displacement is provided by LVDTS, which are coupled with signal conditioners , whose output is between 0-2.5v DC. Also
1)Each DRV would requires 6 PWM signals to drive BLDC motor, so overall I require 6*4=24 PWM signals for 4 actuators.
2) Current control is achieved through PWM so I need a DRV which can give me Phase current feedback for my current control loop.
3) Also with the DSP I should be able to read the hall signals.So the DSP should be able to read 12 hall signals from 4 motors.
4) There are 4 LVDTS and signal conditioners so , DSP should be able to read the 4 analog signal conditioners outputs.
3) I want to develop a GUI with which I would like to see the actual LVDT displacements primarily how ever it will be bonus if I can also display phase currents and speed.
4) In my simulation I measure the speed by taking the derivative of LVDT signals. Would you like to comment on my speed measurement strategy.
my simulations are in simulink so if you want I can send you block diagram of controller and you can advise me weather I can validate my controller with TI products or not.
2. DRV8301 can't measure current. It has gain amplifiers which can be used to amplify the low-side shunt measurement.
4. you can buffer and display your ADC readings through a GUI
this is what I could answer