Maxon EC-2 (2 pole pairs) won't move in lab12a,b with USER_MOTOR_NUM_POLE_PAIRS = 2 ( the correct value since the motor is a 4 pole)
There was an error in USER_IQ_FULL_SCALE_FREQ_Hz from the beginning that prevented system enable, corrected now.
The curious thing is that if I set the motor pole pairs to 4 the motor moves but with wrong speed.
Lab 13x don't work either with the correct pole pairs entry.
If the encoder was wrong connected the motor should not run att all with the worng pole pairs setting or ?
Everything works fine with the 4-pole pairs Teknic motor.
Any ideas ?