Hi,
I have a problem with CCS debugger when I exit the program the via a breakpoint. Or if I restart the program via CCS button.
When I restart the program it start at the correct address but I and up here: No source available for "0x400a2" / No source available for "0x3ff4fa" Are the interrupt table/peripherals reset?
If I leave the program via a breakpoint and reprogram the controller again . Then when I start the controller the controller moved uncontrolled and quite violent. I think the motor tried to go back to is old position. That is quite dangerous. I can solve this by power cycle the controller before programming.
So I think the internal variables aren't properly reset.
So how do I manually reset ALL of the internal variables of the intraspin controller.
Thanks.