Hello,
I use in my project a piccolo F28069 M and drv 8312kit_revD.
I would like to control a torque with BLDC 'BLY172S-24V-4000' and generate an accuracy torque for my application.
I have run lab_2a succesfully, where the identification gives the results : (see file.rar)
Afterwards, I have run lab_5a, The spreadsheet which can be found in the folder:
"C:\ti\motorware\motorware_1_01_00_13\docs\labs\motorware_selecting_user_variables.xlsx " helps me to setup user.h parameters (see file.rar).
Following procedures cited in instaspin_labs (lab_5a) I found gains of the controller exactely the same thing as calculated in calcPIgains(see file.rar).
Spining the motor under a load:
-“Flag_enableSys” true
-“Flag_Run_Identify” true
-Increasing the variable “gMotorVars.IqRef_A”: firstely the force angle is enabled, when the oscillations are above 1Hz the force angle is desabled
Continue to increase the Iq reference I noted how the torque provided by the motor changes (which is logic).
my problem is the appearence of high oscillations (the system will be instable) after a threshold of Iq reference.
I joined my user.h (see file .rar ); where did this instability come from?
Thank you0118.file_lab_5a.zip