Hi,
I wanted to ask here if someone ported the InstaspinBLDC example to the launchpad+booster setup. I want to be able to evaluate it in comparison with FOC using the same hardware.
I understand porting the code it is a non priority for TI http://e2e.ti.com/support/microcontrollers/c2000/f/902/t/398617 because they are pushing everyone to use FOC instead. So I was hoping maybe some user already did the work so that I do not have to replicate it. :)
Regards,
Piotr