Hello, I bought this kit to run our custom 24V/60A motor. I thought it could handle 82,5A but I see here on forum that in practice it is only 28AAC (if sinusoidal)?
Is it just a matter of the 2mohm power resistors, ie can we change these to 1mohm to expand current max?
The mosfets are rated for 120A if I remember? We will also have good cooling of these.