i have an experimental kit motorware software can support it ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i have an experimental kit motorware software can support it ?
hi maria
if i want to implement space vector pulse width modulation on tms320f28027 Piccolo Microcontroller what should i do?
oka i will see these library, i will let u know about it... Kindly send me lab session related to this control, i shall be very thankful to you..
You need to compare between F28027 and F28035.
1. First of all, you need to change the CMD files because their memories are different.
2. F28027 has no QEP, so everything related to QEP in the code should be commented in,
3. F28027 only has 8 PWM channels (compared to F28035 that has 12) so check whether the codes use more than 8 channels of PWM
4. F28027 only has 7 ADC channels (compared to F28035 that has 14) so check whether the codes use more than 7 channels of ADC
5. F28027 only has 20 GPIOs so check whether the using of GPIOs in the code are exeeded the available pins.
I think the rest, they are the same.
Hello, have you read the document qsg_hw_cncd2807f.pdf that can be found in the folder motorware\motorware_1_01_00_14\docs\boards\control\f2802x\docs?
There you can find the information about the switches in this control card. I believe they are the same.