Hi there,
I'm trying to identify a new motor using a LAUNCHXL-F28069M and BOOSTXL-DRV8301 and lab 2b. The process runs smoothly up until it tries to identify the inductance of the motor. When coming out of EST_State_RatedFlux (I think the next step is to identify the inductance) the program will stop and report CTRL_State_Error.
From the spec sheet...
Resistance: 6.2 Ohms (estimated at around 3 Ohms)
Inductance: 49 mH
Wondering if anyone knows what could be causing the error.
Thanks!