I have the DVR8301-69M kit and I'm having a fault latch when running the motor at 17,000rpms in the instaspin motion GUI. At lower rpm's the motor runs just fine, but at 17,000 rpm's and above the DVR8301 pulls a fault and latches. I don't see any fault information in the instaspin GUI. Is there a GUI available that will show me the detailed fault information that is sent from the DVR8301 SPI? Is there an example code composer project that is setup to read and display the fault information reported by the DVR8301?