Hi,
I have a question about USER_MOTOR_MAX_CURRENT user.h setting.
I'm using lab2c for low inductance motor.
First I was running PMSM motor at setting the USER_MOTOR_MAX_CURRENT to 1.0A.
At this time, it was working properly.
In the second I was running PMSM motor at setting the USER_MOTOR_MAX_CURRENT to 3.3A.
At this time, it was not working.
The maximum current of the motor spec is 3.3A, but I run only in 1.0A.
I think that USER_MOTOR_MAX_CURRENT value is not affect the motor action.
Please teach me the reason it does not work at USER_MOTOR_MAX_CURRENT 3.3A .
Best regards,
Mino.M