I’m testing a Marathon AC induction motor #56H17E5303, ½ HP, 4 pole, with the HV Kit.
Using Lab 10b, to reach rated speed (1800 RPM No Load) an over-modulation of 1.33 is needed. Without over-modulation the no load speed is limited to around 1650 RPM.
But with over-modulation the motor becomes unstable with load. Adding load distorts the current waveform and causes the motor to loose speed and sometimes stop. The instability with load is less with less over-modulation, but then the top speed is correspondingly lower. For example, with over-modulation set to 1.10 the motor runs OK at full load, but max speed is around 1690 RPM.
In a previous post Chris indicated that over-modulation works for most motors, but in a handful of cases current samples are too poor to keep stability. He also indicated an updated better over-modulation technique should be in the next MotorWare release.
From my problem description, does it sound like my motor is one of the problem motors?
Any suggestions to make this motor deliver rated speed and torque?
Is there a schedule yet for the next release of MotorWare and will it have the over-modulation improvement?
Thanks.