Hi there,
I'm very new to this TI Launchxl F28069m. I'm trying to find the example of using usb communication, but do not find one. However, I've found the example of usb_dev_bulk for F28069m but not directly for this launchpad. I successfully compile and download the code to the board and connect the usb port from computer to the pin D-, D+ at the pin GPIO27, GPIO26 respectively and issue the command line "usb_bulk_example" but the program can't start because tiusbdll.dll is missing. I think the usb driver "usb_dev_bulk_x86.inf" is not installed. My questions are follows:
1. Do I need the Vbus for this particular example? or just D- D+ are okay?
2. How to install "usb_dev_bulk_x86.inf" ?
Hope any expert can help me on this, thanks.
Veerachai