Dear Sir / Madam
I am working on a steer by wire system. This system is composed of a motor with a gear that moves the wheel. The motor is controlled with InstaSpin FOC (Sensorless speed control). The position of the wheel is measured with an absolute + incremental encoder. A position loop has been implemented in the microcontroller (the loop is closed with the encoder) and it generates a speed reference for the InstaSpin speed control. This encoder can not be used for the motor control (since there are some elastic elements, tolerances,... the wheel position should not be directly derived from motor position ) it just gives information about the wheel position
The steering is a critical system so safety functions and redundancies should be applied in order to achieve the necessary ASIL level. I would like to use the estimated angle as a secondary wheel position sensor. Wheel position should not be directly derived from motor position for normal position control, but it could be OK in case of failure (primary sensor failure). Is there any accesible variable or function with this mechanical position information (like Pos_mrev in lab12a)? I have seen that there is a function called EST_getAngle_pu, but I don' t really know if this is really what I need.
Thank you in advance,
Borja