Hi:
I want to add two ctrl handles to my code. so I write the code like this.
#ifdef FAST_ROM_V1p6
ctrlHandle = CTRL_initCtrl(ctrlNumber, estNumber); //v1p6 format (06xF and 06xM devices)
ctrlHandle1 = CTRL_initCtrl(ctrlNumber+1, estNumber+1);
// controller_obj = (CTRL_Obj *)ctrlHandle;
#else
is there any problem such as the two handle will share some things (such as est handle), or we can use these two handle independently.
by the way, In rom version FAST_ROM_V1p6, the ctrl handle is allocated by the rom(through CTRL_initCtrl), does it mean we cannot
add other member to the control struct pointed by the control handler ?