I have basically copied the BOOSTXL inverter and made a PCB that will plug into my Launchpad 28027F. All pin mappings are the same. Since my inverter operates at 100V, the DRV8301 has been replaced with three 8 pin gate drivers plus a 12V power supply. I have also updated user.h and the BOOSTXL hardware with new voltage parameters for 50V. So my BOOSTXL with Launchpad work very good now running my motor at 50V.
My question is what references do I need to disable for the DRV8301? I see that by commenting out #define drv8301_spi will disable some items. Or will the Launchpad work fine with my new inverter board without any software changes that reference the DRV8301? I am just not sure what software changes are necessary since my inverter PCB does not use the DRM8301.
Thank you!