Hi
I am working on E-Bike with direct drive (gear-less motor) solution using InstaSpin and I an facing the a problem. When the system is enabled, the rotor is already running, for this reason the controller is not able to determine the zero reference position marked in InstaSpin User Guide (spruhj1f). Thus, motor is start to run such as stepper motor.
Can I start-up InstaSpin while motor is running? I already disabled the force angle flag, but the problem stays there
If negative, How do you recommend to enable the system?