Hello,
I'm using Launchpad F28027F with DRV8301 Boosterpack to drive a BLDC motor to 77000 rpm.
The motor has 2 poles, 48V nominal voltage and max speed at 80000 rpm (77400 accordingly to test sheet).
I've modified the hardware to be able to support 48V and with this I got 46500 rpm. Actually, the max speed was achieved with 28V and voltage greater than this not affect the speed. There are some instability for intermediate speeds between 35k rpm and 45k rpm
Attached is the user.h I'm using.
I'm not sure if it is necessary to modify some filter to be able to achieve the 77k rpm.
Please, feel free to ask more information.
Thank you in advance and best regards,
Henrique.