Hello
I'm currently evaluating LAUNCHXL-F28027F for motor driving, but next step is to create a custom board with higher current and voltage and which should fit inside an enclosure.
I will take TI LAUNCHXL-F28027F as a reference design, and when looking the schematics few questions arise.
The emulator XDS100v2 which includes on board USB to JTAG connectivity is only used to debugging and flashing the cpu. So I better not include that to my design. Instead I use that part from LAUNCHXL-F28027F and just make a connector and adapter cable to my new custom board for debugging and flashing purposes, so it is easy to remove, thus saving costs in reproduction.
What methods LAUNCHXL-F28027F offers for controlling motor with user RPM value?, is there a direct potentiometer read, UART control or something else like that ? Is there anything else I should consider on custom driver to avoid conflicts and unwanted behaviour? Is there PCB or schematics recommendations for C2000 or driver itself ?
Looking forward to create my own board !
Thank you!