1.which variable indicate torque output now.
2.could i control the current output with lab12b?
3.does inertia and friction parameter(it identify with no/low load) need changed during system have very heavy load?
4.if i assume that the load is too heavy, so that motor couldn't spin any more. did software will continual increase current output?
in fact, i had increase the load, and motor speed became to 0.my hardware destroyed suddenly.