When the PM motor is acting as a break (trying to slow down the RPM of the load it is carrying), the energy will feed back to the DC link capacitor. Does InstaSPIN FOC control the breaking when the DC Bus voltage reach a user preset level so that you don't get a DC Bus Over Voltage Fault?
In my application, I do not want to add a break controller on the DC bus to dump the energy on a breaking resistor. What I want is a software solution that reduce or remove the breaking so that the DC bus does not go over voltage. Can InstaSPIN FOC do that?
Thank you.
Townes