Hi Chris and all
We have Motorware 14 running on our own "28069M" hardware. We have successfully identified several PMSM motors and I think we understand the process reasonably well.
We have been wrestling with identification of a 1 HP 220 volt 3 phase ACIM. I will give some background and symptoms and then I also have some specific questions.
We have "fiddled" with most of the user.h parameters in order to get the identification to run - but whatever we do - we don't get very "usable" numbers from the process. In particular - we have varied the PWM frequency, the ISR frequency and the following:
#define USER_MOTOR_RES_EST_CURRENT (1.0)
#define USER_MOTOR_FLUX_EST_FREQ_Hz (5.0)
In general - we find that results are more repeatable with higher ISR and PWM frequencies. Still- whatever we do - the numbers we get have rather high magnetization current numbers (around 3 amps) - and the motor (if it spins at all) will not reach full speed. If we manually reduce the magnetization current to around 2 amps - the motor behaves much better. In fact we have empirically adjusted the magnetization current until we have something that works - but this isn't a very satisfactory solution.
A couple of specific questions:
1) The comments and documents tell us that for ACIM we need to enter a calculated number for:
#define USER_MOTOR_RATED_FLUX (0.8165*230.0/60.0)
However - the identification process appears to ignore whatever we put here and makes up its own number. The numbers it produces are usually lower (around 2 V/hz) than we would expect from the recommended calculation (around 3 V/hz) ...
Has the ACIM motor ID process changed so it no longer needs us to input the calculated rated flux?
2) The motor is intended for a fan. We understand we should do the identification under no load - with the fan removed . If we do this - the numbers we get will not allow the motor to spin at all. If we do the identification with the fan attached - we get numbers that allow the motor to spin - though not at full speed. Can anyone suggest why this should be the case.
3) Can anyone suggest why our magnetization numbers are always too high - even when wee ID with no fan attached?
Thanks.
Richard.