Hello all,
I am presently using Motorware for trying out motor control techniques in DRV8312-69M BLDC motor control kit. When I worked with Control Suite, it had something called the DLOG channel which i could tag on to the required ADC peripherals and was able to observe the real time waveforms thereof. DLOG uses some kind of .asm language which I am not able to understand. Can someone tell me if there's a easy way for viewing the adc signals, like inveter pole voltages, currents in Motorware codes within the software itself without using an external oscilloscope.
PS: I could create a array variable in the code and store the values of the currents, voltage. But there's a limitation where I can't create one with somewhere larger array with more than 400 elements. ( so i can't have a real time look).
Thanks in advance :)