Will the TMDSHVMTRINSPIN control the following BLDC Motor
Nemotech Com 700 DC1-00125B
DC 310V 0.67 HP 1.8 Amp
1000 RPM 3P
I am told this motor has 24 pole pairs and uses Hall sensors for position.
thanks
Russell Conner
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the TMDSHVMTRINSPIN control the following BLDC Motor
Nemotech Com 700 DC1-00125B
DC 310V 0.67 HP 1.8 Amp
1000 RPM 3P
I am told this motor has 24 pole pairs and uses Hall sensors for position.
thanks
Russell Conner
How would one connect the 310vdc to the kit, purchase or build a power supply? Is there a cut sheet on the controller showing motor lead connections and bus power input showing allowable voltages? I could not find this in the support material on the TMDSHVMTRINSPIN page.
thanks
Russell Conner
there is a DC input (banana jacks) if you want to bypass the AC input. Yes, you would need a DC power supply.
The documentation for this EVM (TMDSHVMTRINSPIN TMDSHVMTRPFCKIT are the same inverter board) is in controlSUITE at
C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\~Docs