Hi,
I am trying to understand the use of EST_setMaxCurrentSlope_pu() and EST_getMaxCurrentSlope_pu().
The labs do "get" while the motor is not identified, and then "set" of the same value when the motor transitions to identified.
Spruhj1f section 14.4.2.1 indicates the set should be of the maximum value (IQ(127.99).
Why do the labs get the value, then write the same value?
Is the "get" or "set" even necessary if:
1) There is no motor identification or Rs calibration on startup? Just ADC offset calibration on startup.
2) Using SpinTAC move and velocity control?
3) Induction motor?
Should the max value be "set" as indicated in the user guide?
Thanks