MCU- TMS320F28069F
Tools: Code Composer Studio v6, xvds100v2
Hardware: DRV8312EVM Rev D kit
Symptoms: Motor runs at 2500RPM with -2.8 A of Idref_A current. I am only able to increase gMotorVars.Idref_A to any value but in reality only upto 3 A is running from the board to the motor.
What parameters need to be altered to increase the current output?
I will provide files/config info as requested.
Thanks