I am using
F28069M controlCARD
DRV8302-HC-EVM Rev D
controlSUITE3.4.0
motorware_1_01_00_16
CCS 6.2.0.00050
C2800 Compiler Tools 16.6.0
Concern:
these 4 vars:
- GMotorVars.Flag_enableSys
- GMotorVars.Flag_Run_Identify
- GMotorVars.Flag_enableForceAngle
- GMotorVars.Flag _enablePowerWarp
these are showing as unsigned char in the scripting console
as opposed to the page 36 info on lab 2a showing as unsigned int
I get red LEDs on GPIO31 (flashing) and GPIO34 (steady)
Is there some undocumented fix required in the source or a setting?
I am using a BLDC motor (assumes many PMSM settings)
We get errors trying to runGMotorVars.Flag_enableSys =1 and GMotorVars.Flag_Run_Identify =1
thanks
Jim