Other Parts Discussed in Thread: MOTORWARE, CSD19506KCS, DRV8305, DRV8301, DRV832X, TIDM-1003, BOOSTXL-DRV8305EVM, CONTROLSUITE
Hello, I am currently working with a custom built motor that is sinusoidal wound and has very low inductance (approximately 5uF per phase) I also have an encoder I can use with the motor if needed. I am attempting to use the TI controller to test a maximum efficiency point but am concerned that I may not be getting the most out of the motor that is possible. I believe that due to the low inductance of the motor it is not fully smoothing the pwm into sinusoidal control signals. I would like to use some line inductors to add external inductance to assist in this process but am concerned in how this may effect the control. Right now I am not concerned with losses before the motor, I can currently take measurements in between the motor and controller so I can isolate the motor performance.
So some questions
How will external inductance effect the control signals?
Can this be accounted for somehow in the proj_lab code?
What if anything should I change in the code to ensure it is sending a SPWM signal? Or is this default/possible?
Thanks in advance
Jesse