My application is fluid pump controller that has been developed based on Lab10d. The pump works well at 6000 rpm with 20 psi back pressure. When the speed is increased to 7000 rpm or the back pressure is increased to 30 psi, the pump stalls. When either the speed command or the back pressure reduces, the pump was able to resume operation. Attached is the real time watch window data, you can see that the Iq is 5.2A that is below its max setting 15A, and Vq is 0.29 PU. Increasing Kp_Idq does not improve the performance. Please note that we have only two current sensors on phase A and B respectively. Please advise what shall be changed in order to achieve higher driving power.