Following Quick Start Guide: Hardware Setup steps 5-6 I am unable to install usb drivers correctly.
OS: Windows 7
driver is CDM 2.06.00 WHQL Certified, date 12/12/2012
In Windows Device manger under Universal Serial Bus Controllers I only see: Texas Instruments Inc. XDS100 Version 1.0 A
channel B doesn't appear and a com port device doesn't appear.
I have tried a variety of ways to resolve this issue but nothing is helping.
here are some of the links I have followed to no avail:
http://www.ftdichip.com/Drivers/D2XX.htm
and when I tried to enter the part number of this kit, it doesn't show up in the list: TMDSNVMTRKIT5X,
can someone give me a hint on what to do to resolve this issue.
Thanks
Rick